Other Parts Discussed in Thread: SN65CML100, ADS6244
I want to interface the ADC ADS6244 with the DSPTMS320c6455 as I want high speed data capturing for me proto type test equipement. ADS6244 is a 14-bit ADC and having a Serial LDVS output. Can I directly connect it with the SRIO port of the DSP ( or convert it into the CML output suing SN65CML100 ) and store the ADC data in DDR2 RAM (my ADC conversion speed is 105 MHz).