Hi!
I have two questions regarding the ADS4245:
From table 7 in the datasheet, there is a chA standby chB active mode. What about chA active and chB standby, is this available?
I need to shut the ADC down when not in use to save power. I have two options:
a) use the ctrl-pins to enter power down mode.
b) to disable the analog 1.8V power supply.
I cannot find any information in the datasheet regarding power sequencing and whether it is possible to shut down the analog power supply while the digital power (output buffer) supply is still enabled.
please advise!
thank you and best regards
Knut Olav Skyttemyr