This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS1298 - getting the ECG readout

Other Parts Discussed in Thread: ADS1298

Hello TI community,

We are evaluating the ADS1298 converter for our product. We've managed to establish the connection with the board using SPI interface driven by AVR32 microcontroller.

It took a while before we could read the test signals - it was not possible to use the default settings and only change the channels input type.

Shortly, if I set the registers with the following values:

CONFIG1 (0x01): 0x85 or 0x06 (default)

CONFIG2 (0x02): 0x10 (default is 0x0)

CONFIG3 (0x03): 0xDC (default is 0x40)

LOFF (0x04): 0x03 (default is 0x0)

and all the channels to test signal (0x05) - I get nice test signal. If I now switch the channels back to the normal input (0x0), I don't see the signals I am feeding the ADS1298 with. We are using the LionHeart 2 patient simulator that can generate ECG-like signals with the real-life amplitudes.

My question is - which registers should I change to enable the ECG reading? If we use the ADS1298/8R EVM evaluation software, the ECG traces are read. Using the same registers settings in our software gives no results.


We've also checked the SPI communication with an oscilloscope - everything looks well, only the ADS1298 is not sending reasonable data back.

Any help will be greatly appreciated.

Best regards,

Mike