Hi,
Is it possible to interface LM97600 with GTP transceiver (SX series) instead of GTX of Vitex-5 FPGA?
What is the maximum no. of samples/ch that can be acquired in LM97600RB in 4-channel mode in a single shot?
Best Regards,
Supratim
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
Is it possible to interface LM97600 with GTP transceiver (SX series) instead of GTX of Vitex-5 FPGA?
What is the maximum no. of samples/ch that can be acquired in LM97600RB in 4-channel mode in a single shot?
Best Regards,
Supratim
Hi Supratim
The GTP transceivers may not be fast enough to capture the LM97600 output data. The data rate is 2x the applied CLK rate, so for a CLK of 2500 MHz each lane is outputting data at 5Gbit/sec. I believe GTX transceivers will be required to support this data rate.
The LM97600RB can capture up to 4Msamples for each channel when operated in Quad input mode.
Best regards,
Jim B