Other Parts Discussed in Thread: THS8200, AM3359
Hi All,
We are using THS8200 IC for converting LCD parallel signal to VGA on phyBOARD-WEGA-AM335x(SOC AM3359).
On VGA monitor we are getting on vertical stripe.
If i moves the QT application to that area, shadow is coming on the VGA monitor.
Please find attached jpg for problem.
I am using below XGA resolution.
XGA 1024 x 768 @ 60 Hz pixel clock 65.0 MHz
Horizontal Timing (pixels) Vertical Timing (lines)
Visible area 1024 768
Front porch 24 3
Sync pulse 136 6
Back porch 160 29
Whole line/frame 1344 806
Bellow are the register values of THS8200 IC.
*************************************************************************
DATASET_NAME,"DMT ID: 10h, 1024x768 @ 60Hz, 48.363kHz, 65.000MHz, HS/VS -/-, RGB 444 DS>VGA, THS8200"
//THS8200
INCLUDE,THS8200_RGB_444_DS_to_VGA_common.inc
register value
WR_REG,THS8200,0x01, 0x34, 0x05 // dtg1_total_pixel_msb
WR_REG,THS8200,0x01, 0x35, 0x40 // dtg1_total_pixel_lsb
WR_REG,THS8200,0x01, 0x39, 0x33 // dtg1_frame_field_msb
WR_REG,THS8200,0x01, 0x3A, 0x26 // dtg1_frame_size_lsb
WR_REG,THS8200,0x01, 0x3B, 0x26 // dtg1_field_size_lsb
WR_REG,THS8200,0x01, 0x70, 0x88 // dtg2_hlength_lsb
WR_REG,THS8200,0x01, 0x73, 0x07 // dtg2_vlength_lsb
WR_REG,THS8200,0x01, 0x82, 0x40 // dtg2_cntl, RGB mode, discrete syncs
regards,
syed