Other Parts Discussed in Thread: DAC9881
Dear members.
I can't find definition sampling rate(fDac) of DAC in any data sheet and other web site.
Please teach me definition as equation.
eg; fDAC = xxx /***
regards,
Kenji Itoh
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: DAC9881
Dear members.
I can't find definition sampling rate(fDac) of DAC in any data sheet and other web site.
Please teach me definition as equation.
eg; fDAC = xxx /***
regards,
Kenji Itoh
Kenji,
This depends on whether you require the output to fully settle or not. You can write the a give DAC as quickly as the digital interface allows you to, but the output may not settle.
If you want the output to settle, the update rate is simply the settling time specification.
Here's a blog post if you'd like to read more about settling time:
http://e2e.ti.com/blogs_/b/analogwire/archive/2013/08/26/dac-essentials-understanding-your-dac-39-s-speed-limit.aspx
Kevin-san
Thanks your reply. I understand settling time in DAC.
But I want to answer how set up equation sample rate of DAC in datasheet.
For example, settling time of DAC9881 is 5 micro sec. But it's has no sample rate (fDAC).
And my customer asked sample rate (fDAC) of DAC9881.
Regards,
Kenji itoh
Kenji,
An ADC has an analog input and a digital output and the conversion process takes a finite amount of time to deliver the digital output word, which is provided in all ADC datasheets as the sampling rate.
A DAC, on the other hand, has a digital input and an analog output. Our result is analog which has an infinite number of possible states, as compared to the finite number of states of a digital output. In this case the output is updated immediately once the digital word has been latched to the DAC data register, however it takes some time for the analog output to slew and settle to the value it was programmed to. In this case the datasheet provides the worst-case amount of time it would take for the DAC to settle over a very wide step and settle within some specified error band, usually 1/2 the LSB weight.
This means "update-rate" or sample rate (sample rate is really a bad name for this mechanic related to a DAC - we're not really sampling anything. We're writing. Updating) for a DAC has some room for interpretation, unlike the ADC that delivers a very specific result with very specific timing. In one case it could be defined by what is the maximum rate with which we may write to a given part. In this case the update rate is defined by the digital interface timing requirements. In the other case, if we required fully settled analog outputs, the sampling rate is defined by the settling time.
Does this make sense?