Other Parts Discussed in Thread: DAC3482, LMK04828
Hi,
Attached is a simple block diagram re DAC3482 drive issue from a customer of ours.
The customer is using the DAC3482 in a non-standard way, because they need to use gated (non-DC balanced) signals on the DACCLK and OSTR pins. The datasheet requires AC coupling this signal which they therefore cannot do.
The ? is the circuit in question on the attached that cannot be a capacitor as the DACCLK and OSTR cannot be DC balanced signals in their application.
They tried with LVPECL buffers using negative supplies as the ground to level shift the signals but this approach has fallen through.
Could anyone assist here to resolve this issue?
Thanks.