Hi,sir:
There is an issue with ADS1118EVM,detail issue description as below.
When ADS1118EVM softwave is running,It creat a curve about 26℃,7uV~24uV at normal.
But it create a high temp curve (about 650℃,26mV) when drag the running ADS1118EVM window.
We discovery the high temp curve can be show when dragging the softwave window.
We have some experiment with 8SPS、16SPS、32SPS、64SPS、128SPS、250SPS、475SPS、860SPS .The high temp curve is alway show with 8SPS . The high temp curve is show sometimes with 16SPS、32SPS. The high temp curve is never show more than 64SPS.I consider maybe the issue source from the ADS1118EVM softwave,but I can’t sure it.
Any suggestions for how to solve the issue on this ADS1118EVM would be greatly appreciated.
Thank you.