This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SD303EVK, SDI Output issue



Hi,

I have purchased SD303EVK for SDI evaluation. I am driving differential SDI (Color Bar) into SMA inputs but see no outputs from BNC connector. I am using the board that has only 1 side BNC populated. The SDI Output is connected to the Scope and the compliment of it is terminated with 75Ohm termination. I know that the RealTime Scope is 50Ohm but all I am trying to see is some kind of output wiggling. The SDI patter is generated by Tek WFM2300 Waveform Monitor.

Thank you