This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS1120 / supply current in single-shot mode

Guru 29720 points
Other Parts Discussed in Thread: ADS1120
Hi Team,
 
My customer considers to use ADS1120 in single-shot mode to reduce power consumption.
Is there any supply current data in single-shot mode?
He would like to know the value under DR=600SPS(normal mode) and gain=128.
 
Best Regards,
Yaita / Japan disty
  • Hi Yaita,

    The currents for IAVDD and IDVDD are shown on page 5 of the datasheet.  When the START command is issued relative to the last SCLK falling edge of the START command (this is explained on page 26 of the datasheet), there will be 6994 tclk periods (Table 7) until the conversion completes and the device returns to sleep (when in single-shot mode).  When using the internal oscillator the tclk period is 1/4.096MHz.  This means the conversion will take about 1.708ms to complete.  Also when using the internal oscillator you must add an additional 50us of on time for the oscillator to start and settle.  So on time calculation will be about 1.785ms with 510uA for IAVDD, and off time the current is about 0.1uA typical.  The IDVDD is 75uA typical during the on time and 0.3uA typical during the off time.  Remember however that these values are only for the conversion and do include the IDAC currents if used. 

    Best regards,

    Bob B

  • Hi Bob-san,
     
    Thank you for your detail&clear explanation.
    I appreciate for your support.
     
    Best Regards,
    Yaita