Hi
I was wondering if it would be possible to get the HLD code for this ADC. Also is possible to set up and automated run on this ADC (for example using a python code to test different input frequencies)
Thanks
Jill
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
I was wondering if it would be possible to get the HLD code for this ADC. Also is possible to set up and automated run on this ADC (for example using a python code to test different input frequencies)
Thanks
Jill
Hi Jim,
Yes I am looking for the VHDL code used by your capture card. The mode I'm using is the bypassing mode. And the FPGA was just planning on using the one that on the data capture board (ArriaV 5AGME1EH29).
Thanks,
Jill
Jill,
The link below will provide the firmware that was generated with the MTI JESD IP core. We are currently working on a new build that will use the Altera Mega-core JESD IP. This shoud be available in about 1 month.
Regards,
Jim