This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS1292 Error Code 8

Pl tell me if we connect 4 lead ecg cable from patient to demokit db 9 connector and also connect to Mini usb to laptop then 3 terminals analog & digital  voltage are required for live ecg or any software operation.

Here also when software window open the error window show " An error occured with error code 8. create folder in ads1292x9xEVM_main.vi<APPEND>D:\program files\Texas Instruments\ADS1x9xevm\saved". what is this problem.pl give me sol. I have purchased for research purpose. Pl tell me what expriments we can do on this kit.

Thanks Rakesh

  • Hi Rakesh, 

    This error occurs when the listed directory does not exist. The installer tries to create this directory, but sometimes Windows 7 permissions prevent it from doing so.

    You should be able to navigate to "D:\program files\Texas Instruments\ADS1x9xevm" in Windows Explorer and create a folder called "saved" to resolve the issue.

    The EVM is powered from the USB supply, so you will not need to connect any additional power supplies to operate it.

    Regards,