Hi,
I have a DAC161S997EVM board that I'm having trouble with, for a start when I first got the board it would not connect to the PC to run the demo that comes loaded. But I didn't consider this as too much of a problem, I'll program it myself. That's where I started to have trouble, when trying to program the board from CCS I get an "Unknown device" error. The TJAG (MSP-FET430UIF) is connected through the J2 header in the correct orientation and the board is powered by the loop when tying to program. I can't work out whats wrong Is there a jumper that needs setting for programming or something? Any help appreciated
Nick