Other Parts Discussed in Thread: ADS1298
During the installation of the latest software posted on ti-web site (ads129xecg-fe-setup-1.1.1.exe), and during the portion of the installation of the device driver software, the following error dialog window appeared : "There was a problem starting libusb0.dll - The specified module could not be found." The installation of the software did however complete "successfully" and the evaluation application was able to be started, however the software behaves inconsistently sometimes saying it can't connect and "reset firmware", and other times it will connect but say "DSP not ready ..." - additionally the software will behave the same way even if if there is NO MMB0/ADS1298 hardware plugged into the USB port. My conclusion is that the USB-driver software did not install correctly - is this a known issue and if so is there a "fix"? Running Windows-7 64-bit with all recent software patches from Microsoft installed. Tried installing on two different Windows-7 PCs with same result. Hardware being used is MMB0-REV_D and ADSIx98ECG_FE_REV_C . Any suggestions appreciated as right now all I have is two $200 unusable circuit boards.