Hi team,
How do I change the NCO frequency for the ADC12J4000? Do I just use the GUI's NCO configuration tab? Irrespective of the values I enter on the GUI, the NCO is always set to 75% of the sample clock frequency (I am basing this comment on the observed output signals).
The ADC registers are set automatically by the GUI (High Speed Data Converter Pro GUI), but there is no documentation on the registers, so even though I can see the bit values in the registers, I don’t know what they mean.
Could you please provide the documentation of the registers?
Best regards,
Max