Hello,
I read in datasheet that input scale and LVDS interface is controlled by SPI.
Can I set those without SPI?
If I do not use SPI, what is the default setting value?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
I read in datasheet that input scale and LVDS interface is controlled by SPI.
Can I set those without SPI?
If I do not use SPI, what is the default setting value?
Hi Kim,
The only way to change the input scale and LVDS interface from the default is through SPI.
The default value for input scale is 2Vpp and the LVDS interface is QDR mode.
Thanks,
Eben.