I am using the ADC12J4000EVM together with the TSW14J56EVM. The SW I use is High Speed Data converter Pro 2.6, together with the ADC12J400EVM GUI version 1.3
Running with an internal clock -- the lowest frequency I can set up the ADC12J400EVM using GUI version 1.3 is 1966.8MSPS. If i want to set it up to a lower sampling frequency, how should I do it? Can this be done via the specific configuration of the chip registers?
Thanks
Boaz