Hello, i'm trying to use AFE4300 to measure weight, using external load-cells. Do you have any detailed instruction for weight-scale function like the SBAA202 for impedance measurement?
And in the BOM, what is the use of R95, R96, R97, R98?
Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello, i'm trying to use AFE4300 to measure weight, using external load-cells. Do you have any detailed instruction for weight-scale function like the SBAA202 for impedance measurement?
And in the BOM, what is the use of R95, R96, R97, R98?
Thanks
An,
Unfortunately we do not have any additional documents describing how to use the weight scale other than the user's guide and that datasheet.
Those resistors are part of the anti-aliasing filter on the input. This is found on the weight scale input signal page of the schematic found on page 40 of the user's guide.
Hello, thank you for your answer.
I just found something related to weight-scale function in the demonstration code AFE4300EVM-PDK, and i have some other questions:
1. In the MSP430F449_AFE4300Controller.c file, line 462, it was written:
spiWrite(0x09,0x0005);
It means DEVICE_CONTROL1[14:13] are set = 0b00. But in the datasheet, it is said that "Not used. Always write 1".
Can you explain me the difference here? What happens if the "not used" bits are not set correct?
2. At line 458, it was written:
spiWrite(0x0D,0x003F); // Max Gain, DAC to "Zero"
As i understand from the datasheet, the OFFSET_DAC_VALUE[5:0] were set = 111111, means -1 x 31.2mV offset correction. How could it be "Zero" like the comment?
3. Line 461, spiWrite(0x01,0x4143);
so ADC_CONTROL_REGISTER1 bits[3:0] were set = 0011, but in the datasheet it is said: "Always write 0000. At power up, these bits are set as 0011". So one has to set the bits as 0000 or 0011 ?! I thought it implies after power up, the bits are automatically set as 0011, and one has to rewrite them by 0000?
Thank you
An,
Our software is given as a starting point to customers and is given as is.
1. This sets the DEVICE_CONTROL1 register to power up the front-end, power down the BCM, and power up the weight scale. Bits 2,1,0 respectively.
2.The comment is a typo
These bits set the value for the DAC used to correct the input offset of the weight-scale front-end. The correction is made at the second stage. The offset correction at the output of the first stage is given by OFFSET_DAC_VALUE x 31.2 mV. Note that OFFSET_DAC_VALUE is a number from -32 to 31, in twos complement; default is ‘000000’.
3. We just set them to the power up defaults.