Other Parts Discussed in Thread: MSP430F5529, ADS1298
Hi, i´ve my MSP430F5529 launchpad connected to the ADS1298 EVM and i´ve a couple of doubts, first when i configure DCO=8MHz and SMCLK=4MHz for the SPI, i can write and read the Registers of the ADS1298...but when i set a channel to "power down" option with the channel register i still read some values for this channel, and the datasheet indicates that it should be zero...could be it noise? or there is some wrong with the registers?
Example of a reading "[C0 00 00] [00 0A FE]......."
And the secondone, when i change the DCO=25MHz, the SPI communication only works with the register UCB1BR0=36, and i can only read and write registers when DRDY toogles there are zeros for all measures...i dont understand why this happens, i use the formula: fBitCLK=(fBRCLK/UCBRx+1); and the value is between 110kHz and 20MHz that stablishes the datasheet....
Any help will be welcome!