Other Parts Discussed in Thread: ADS1278, THS4531A, THS4521
Hello,
I'm using the ADS1278, and I'm wondering if I can get away with using the THS4531A instead of the THS4521 because of it's lower bias current. I intend on using a 40kHz data rate in low power mode for the ADC, the THS4531A has a lower bandwidth (36MHz vs 145 MHz); I wonder if it's good enough?