SCLK serial output clock on ads1278 what option would work with a ftdi USB out chip to interface to the ads1278?
I am looking at AN_108 command processor for the mpsse & host bus emulation mode from the ftdi site for the ft2232 chip.
6.11, 6.12 section of that sheet has two options that look like they work for DRDY data ready does the clock have to stop can it keep going?
I am trying to find a configuration option that would work...
they are for clock for nx8 bits with no data transfer until GPIOL1 is HIGH, or LOW depending on the opcode.
So if you could help me out here that would be great.