Dear all,
I am looking to use the ADS1220 in an application that is pseudo-differential with AIN1 = 0.25V - 4.75V and AIN2 = 2.5V. Both AIN1 and AIN2 are ratiometic to supply (AVDD = 5.0V, AVSS = 0V), with VREF = 2.5V, via a voltage divider.
According to Equations 4-6 (p19), this meets the common-mode voltage requirements for the sensors with the PGA enabled.
The datasheet does not place any constraints on the absolute value of AIN when the PGA is enabled - only when the PGA is disabled. Are there any constraints that need to be observed, even if specific to the voltage range in this application?
Also, with regards to the reference, the datasheet states the following (with added emphasis):
"The reference inputs are internally buffered to increase input impedance. Therefore, additional reference buffers are **usually** not required when using an external reference and the reference inputs do not load any external circuitry when used in ratiometric applications."
Is there any further guidance for the reference on this device? Are there any further recommendations for filtering on the reference?
Thank you in advance for your help,
-- Damien