This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Connect ADS1248EVM on MMB0

Other Parts Discussed in Thread: ADCPRO, ADS1248

Hello, i would like to know if it's possible to connect an ADS1248EVM to an MMB0 ?

I try to do it but it doesn't work ... May be someone could help me !

What I've done is :

1- Power up the MMB0 with a 6V wall mount and a +/-10V on the pins +VA and -VA

2- Plug the ADS1248EVM on the MMB0

3- Install ADCPro

4- Install ADC PRO plugin for ADS1248EVM

5- Install driver from the plugin install

6- Connect the usb cable

For windows my device is an unknow USB device and when I launch ADCPro he doesn't find my device.

Is someone has a solution ?