Other Parts Discussed in Thread: ADS1243-HT
I need some help figuring out the conversion rate I should be expecting from the ADS1243-HT. I am clocking it at 1.25 MHz, 3.4V, DR0 DR1 = 00, SPEED = 0, gain = 1 or 16. It seems that the datasheet indicates conversions should happen at 15 Hz, so one would take 67 ms. For me, conversions are taking anywhere from 255 to 377 ms. Does that sound reasonable, and do you have any suggestions on speeding this up?
Thanks
Ron