Hello,
I am planing to buy an AD converter DC12D1800RF for a project. The purpose of project is to precisely measure the phase difference of two very high frequency signals. The frequency of two input signal is about 1Ghz.
In order to measure the phase difference of two input signals, first, the input signals (analog signals) are connected and sampled by two corresponding ports of the AD converter. Then the sampled signals are loaded to the computer for processing (band-pass filter for instance). The processed signals are integrated with each other for measuring the phase difference.
Because the sampling rate of the AD converter is 1.8Ghz, this means there will be about 1.8Ghz x 12 bits data read and acquired by the computer in 1 second. The amount of data is too large to process.
So my question is how sampled signals are read to the computer and is it possible for me to measure the phase of two 1Ghz signals using DC12D1800RF?
Please help,
Sincerely,
Quang.