Hi ,
I am using ADS7958SRGET in my design. I have few queries listed below.
1. Is it possible to power-up the device via in-band signalling (SPI Frame) ?
2. Can system-level soft-reset be asserted (via in-band signalling) ?
3. If the control registers get bombarded with random bit patterns, is there any likelihood that the device can go into an un-recoverable state? OR
4. Are there any hidden (unpublished) SPI accessible registers (like when device is used in TI’s internal testing / debug / manufacturing environments) which may get effected when control registers get bombarded with random bit patterns.