This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADC12J4000 4GSPS

Other Parts Discussed in Thread: ADC12J4000, LMX2581, ADC12J4000EVM, TRF3765, LMK04828, LMK00301

Hi all,
My customer plans to use 8 units of  ADC12J4000, and has some questions.

1. ADC12J4000EVM uses LMX2581 for ADC sampling clock and its sampling rate is upto 3.76GHz.
   When ADC sampling clock is 4GHz, what device is recommended?
   Also, is there the 4GSPS based reference circuit like ADC12J4000EVM?

2. When using 8 ADC's which are connected to one FPGA and all ADCs are synchronized,
     are there any recommend clock ICs and the clock tree for this application?

I am happy to receive any advice on the design.

Regards,
Toshi