Other Parts Discussed in Thread: ADS1258
I am using the ADS1258 to read an input signal which when open circuit, is terminated with a 499kohm resistor to 0V so that it does not float. The mux input leakage current is not specified for this device so I assumed a typical 10nA.
However, we are finding that at low temperature and room temperature this is fine, but at +70degC, it is very large. For assemblies up to now, it was less than 100nA but the last batch of parts showed up to 150nA which is failing our test limits.
Is there any data for this parameter?
Note that the MUX output is opamp buffered to the input of the ADC.