Other Parts Discussed in Thread: ADS7822
Dear All, this is my first post. I hope writing on the right section.
My target is to measure analog source which is between 6mV to 40mV.
Instead of using op-amp (which means a lot of noise or a lot sampling for me & I need 3 opamps, because I need 3 different readings) I'm using x3 ADS7822 with 400mV vref supplied by LT6650. I have 400mV/4096 resolution and noise reduction with relatively less cost.
Microcontroller is MSP430 and code developed with CCS energina.
The problem is; I have the source measured 6.6mV. However adc reading I received is '73'.
400mV divided by 2^12 (4096) is 0,09765625
73 * 0,09765625 = 7.12mV
There is some difference on the measurement. Are there some problem on the adc reading code? I tried with 377mV source and the adc reading was 3640.
Here is the code;
long int get_ads()
{
long int data = 0;
short int delay_time = 1;
//Start new conversion Cycle
digitalWrite(P1_5, HIGH); // set CS high //PIN_SET(ADS7822_CS);
delay(2);
digitalWrite(P1_5, LOW); // set CS low //PIN_CLEAR(ADS7822_CS); // enable ADS7822
digitalWrite(P1_6, LOW); // set CLCK low //PIN_CLEAR(ADS7822_CLK);
delay(1);
// first 3 bits
for(int k=0; k<3; k++)
{
digitalWrite(P1_6, HIGH); // set clk high
delay(delay_time);
digitalWrite(P1_6, LOW); // set clk low
delay(delay_time);
}
for (int c = 0; c < 12; c++)
{
if(digitalRead(P1_4) == HIGH) data |= 0x0001;
if(c < 11) data <<= 1;
digitalWrite(P1_6, HIGH);
delay(delay_time);
digitalWrite(P1_6, LOW);
delay(delay_time);
}
digitalWrite(P1_5, HIGH); // set CS high disable ADS7822
delay(delay_time);
return data;
}
many thanks,