Other Parts Discussed in Thread: ADS1248
we have a problem with a board from one of our customers that uses the ADS1248 ADC.
Our task is to make a redesign of the board to improve the measurement performance.
The current board is well designed and uses REF5025 reference sources.
When measuring in single ended mode and 5SPS we have a noise of max. 25 ADC counts (about 7,5 µV).
This would be ok for the application, but the measured value has a voltage dependent error.
When doubling the input voltage the error is doubling too.
For example:
|
Input Voltage |
Calculated |
Measured |
Error |
|
203,46 mV |
682.698 |
682.669 |
-29 |
|
806,91 mV |
2.707.541 |
2.707.338 |
-203 |
|
1445,40 mV |
4.849.958 |
4.849.453 |
-505 |
(The measured value is an average of 50)
When using faster sample rates this problem becomes worse too.
Also the self-calibration function of the ADS1248 didn’t solved the problem.
Can you explain this problem?
Thank you for your help.