Other Parts Discussed in Thread: ADS1601
e2e,
We have a customer using the ADS1601 with the following problem:
We’re using the ADS1601. It is set up for the internal reference, i.e. /REFEN (pin 13) is low (pulled low by the internal pull-down). I attached the schematic.
That should make the reference about 3 V, but it’s more like 0.9 V. I’m measuring about 3 V on REFP, and 2.1 V on REFN. It varies from one part to the next, but they are similar.
Other than that, the ADC works, but it makes the full-scale range rather small. The ADC works and produces reliable data; it’s just the reference that’s wrong.
What could be causing the reference voltage to be wrong. I have attached part of their schematic.
Thanks for your help.
John Wiemeyer 2068.ADS1601 Schematic.pdf