This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Interfacing of virtex-6 FPGA board with DAC34SH84 and ADS54RF63

Other Parts Discussed in Thread: CDCE62005, DAC34SH84

Hello!

Even though there are posts related to this topic and read them, not able to figure out what is the problem is my setup.

What I have been doing is as follows

1. Giving a input signal of 2 MHz and a clock of 48MHZ to ADC.

2. The digital data coming out of ADC is being written if a FIFO (which I have defined in FPGA) with write clock of 96 MHz which is the output of MMCM block(1) in FPGA, and the input to this MMCM block(1) is coming from ADC itself (Same clock of 48 MHz that is provided to ADC as clock).

3. Reading the FIFO with a clock of 96 MHz which is the output of another MMCM block(2) in FPGA and input to this MMCM block(2) is coming from the DAC board.

4. The output of MMCM block(2) is also being used for DATA_CLK for DAC.

In short there are two MMCM block in my design and and I am feeding them from different clocks.One clock  is coming through ADC (generated from High frequency function generator) and other is coming through DAC which is generated by CDCE62005.

And I am using FMC connectors to connect ADC and DAC to FPGA board.

Problem is: I am not getting any signal at the output of DAC, which is  expected to be 2 MHz signal that I feed to ADC. I wanted to  attach the DAC configuration file as well as VHDL code. but there is no link where i can do so.

Please help!

Regards

Pramod singh

  • Hi Pramod,

    It will be good to independently confirm that the DAC to FPGA interface works before piping data from the ADC to the DAC. I will also suggest that you follow the recommendations in the thread below to confirm that the DAC34SH84 works.

    http://e2e.ti.com/support/data_converters/high_speed_data_converters/f/68/t/359131.aspx

    Thanks,

    Eben.

  • Hello Ebenezer!!

    Thanks a lot for your quick reply. Your suggestion worked quit well, I  went through the link you have provided and it was ver y useful. It seems DAC is got configured well now. I got some output but not exactly that I am expecting. The signal I am getting is  quit noisy and distorted. Bellow is the waveforms that i am getting.

    The yellow one is the output that I am getting out of DAC, and green one is the input that I am feeding to ADC.

    I am totally blank why this output is like this even though I have considered setup and hold time as well. Can you please suggest me what changes  i can make to get expected waveform. I am attaching VHDL code .ucf file and DAC configuration GUI file here that I am using.Please help.

       x00	   x009C
       x01	   x100E
       x02	   x0000
       x03	   xF000
       x04	   xBFFF
       x05	   xB860
       x06	   x2800
       x07	   xFFFF
       x08	   x0000
       x09	   x8000
       x0A	   x0000
       x0B	   x0000
       x0C	   x0400
       x0D	   x0400
       x0E	   x0400
       x0F	   x0400
       x10	   x0000
       x11	   x0000
       x12	   x0000
       x13	   x0000
       x14	   x0000
       x15	   x0000
       x16	   x0000
       x17	   x0000
       x18	   x20F7
       x19	   x2074
       x1A	   xAC20
       x1B	   x0800
       x1C	   x0000
       x1D	   x0000
       x1E	   x1111
       x1F	   x1144
       x20	   x1101
       x22	   x1B1B
       x23	   xFFFF
       x24	   x0000
       x25	   x7A7A
       x26	   xB6B6
       x27	   xEAEA
       x28	   x4545
       x29	   x1A1A
       x2A	   x1616
       x2B	   xAAAA
       x2C	   x0000
       x2D	   x0004
       x2E	   x0000
       x2F	   x0000
       x30	   x0000
       x7F	   x0000
    CDCE62005 Registers
    Freq:0.000000MHz
    Address	Data
    00		00400000
    01		81840321
    02		80120302
    03		C1840303
    04		C13C0304
    05		000C1A85
    06		84BF2AF6
    07		151877F7
    08		20001808
    library IEEE;
    use IEEE.STD_LOGIC_1164.ALL;
    use IEEE.NUMERIC_STD.ALL;
    use IEEE.STD_LOGIC_signed.ALL;
    Library UNISIM;
    use UNISIM.vcomponents.all;
    
    entity adc_to_fifo is
    port(
    
    	-- inputs from the ADC --
    		-- Data
    	adc_inp			: in std_logic_vector (11 downto 0);
    	adc_inn			: in std_logic_vector (11 downto 0);
    	
    		-- Data Ready (Clock from ADC)
    	dry_clk_inp			: in std_logic;
    	dry_clk_inn			: in std_logic;
    	
    		-- Ref 200MHz clock
    	SYSCLK_P		: in std_logic;
    	SYSCLK_N		: in std_logic;
    	
    	
    		-- FPGA clock from DAC
    		-- FPGA clock from DAC
       fpga_clk_inp	: in std_logic;
    	fpga_clk_inn	: in std_logic;
    	
    	-- 2.11 starts
    	PARITYP			: out std_logic;						--PARITYABP: Sync the FIFO pointer or act as a parity input for the AB-data bus
    	PARITYN			: out std_logic;
    	SYNCP		    : out std_logic;	--SYNCP: allow complete reversal of the data interface when setting the rev_interface bit in register config.
    	SYNCN			: out std_logic;
    	FIFO_ISTRP		: out std_logic;						--ISTRP: act with SYNC, PARITY.
    	FIFO_ISTRN		: out std_logic;
    	
    		-- Data clock to DAC
    	DATA_CLKP		: out std_logic;						--DATACLKP: LVDS positive input data clock. Data are lutched on both edges of DATACLKP/N.
    	DATA_CLKN		: out std_logic;
    	
    		-- SMA out for clock to ADC
    	sma_outp			: out std_logic;
    	sma_outn			: out std_logic;
    	
    	-- output to DAC
    	IO_DAP			: out std_logic_vector (15 downto 0);		
    	IO_DAN			: out std_logic_vector (15 downto 0);
    	-- 2.11 ends
    	
    -- #2.8 	led_1, led_2			: out std_logic; removing led_1, led_2 from output
    	led_out        : out std_logic_vector (7 downto 0);		-- for counter
    	rst            : in std_logic
    	
    --	fifo_rst_in : IN std_logic;
    --	wr_en_in, rd_en_in : in std_logic; #2.10
    			
    -- 2.11	fifo_out	: out std_logic_vector (11 downto 0) 
    	
    );
    end adc_to_fifo;
    
    architecture Behavioral of adc_to_fifo is
    
    -- ----------------------------- Constants ---------------------------
    
    	constant Low  			: std_logic	:= '0';
    	constant High 			: std_logic	:= '1';
    	constant LowWord		: std_logic_vector (4 downto 0) := "00000";
    
    -- --------------------------------------------Component Declaration ------------------------------------------------------------------------
    	
    	
    	COMPONENT counter1 is
    	port(
    		CLK1_counter : in std_logic;
    		LED_counter : out std_logic_vector(7 downto 0);
    		RESET : in std_logic
    		);
    	END COMPONENT;
    
    
    
    COMPONENT fifo_generator_v9_3
     PORT (
        rst : IN STD_LOGIC;
        wr_clk : IN STD_LOGIC;
        rd_clk : IN STD_LOGIC;
        din : IN STD_LOGIC_VECTOR(11 DOWNTO 0);
        wr_en : IN STD_LOGIC;
        rd_en : IN STD_LOGIC;
        dout : OUT STD_LOGIC_VECTOR(11 DOWNTO 0);
        full : OUT STD_LOGIC;
        wr_ack : OUT STD_LOGIC;
        overflow : OUT STD_LOGIC;
        empty : OUT STD_LOGIC;
        valid : OUT STD_LOGIC;
        underflow : OUT STD_LOGIC
      );
    END COMPONENT;
    	-- ------------------------------------------------Signal declaration---------------------------------------
    
    	-- #2.8 
    	--Debug Nets
    	-- signal ovr_in_s : std_logic;
    	signal debug_signal1	: std_logic_vector(11 downto 0);
    	signal led_1, led_2 : std_logic;
    	signal dry_clk_s, dry_clk_2x 		: std_logic;
    	signal clkout4pin, CLKFBOUTpin, CLKFBOUTBpin, CLKFBINpin: std_logic;
    	signal clkout4pin_1, CLKFBOUTpin_1, CLKFBOUTBpin_1, CLKFBINpin_1: std_logic;
    	signal data_clk, data_clk1, pwrdwn	: std_logic;
    	signal sync, fifo_istr, parity		: std_logic;
    	signal    countER     				: integer range 0 to 1:=0;
    	
    --	signal	fpga_in						: std_logic_vector (11 downto 0) := (others=>'0');
    
    	signal	IO_DA						: std_logic_vector (15 downto 0) := (others=>'0');
    	
    	-- checking
    	--signal 	led_out_1,led_out_2			: std_logic_vector (7 downto 0);
    	
    	signal ref_200_clk_s, ref_clk200_bufg	: std_logic;
    	signal dry_clk_delayed_s, dry_clk_bufio_s, dry_clk_bufr_s,dry_clk_bufg_s	: std_logic;
    	signal adc_data_s, data_delayed_s, fifo_out	:std_logic_vector (11 downto 0) := (others=>'0');
    	signal	rst_adc, Ready_idelay_out	: std_logic;
    	signal ff_data : std_logic_vector (11 downto 0);
    	signal full, wr_ack, empty, overflow, valid, underflow : std_logic;
    	signal fpga_clk_s	: std_logic;
    	
    	-- 2.10 
    	signal fifo_rst, wr_en_in, rd_en_in : std_logic;
    	
    	signal led_out2, led_out3 : std_logic_vector (7 downto 0); -- 2.11
    	
    	signal clkout0pin, chip_780_clk : std_logic;--2.14
    	
    begin
    
    	IBUFGDS_inst_refclk1 : IBUFGDS
    	generic map (
    	DIFF_TERM => FALSE, -- Differential Termination
    	IBUF_LOW_PWR => TRUE, -- Low power (TRUE) vs. performance (FALSE) setting for refernced I/O standards
    	IOSTANDARD => "DEFAULT")
    	port map (
    		O => ref_200_clk_s, -- Clock buffer output
    		I => SYSCLK_P, -- Diff_p clock buffer input (connect directly to top-level port)
    		IB => SYSCLK_N -- Diff_n clock buffer input (connect directly to top-level port)
    	);
    
    	-------------- BUFG for ref_200M ---------------------
    	BUFG_clk200inst : BUFG
    	port map (
    		O => ref_clk200_bufg, -- 1-bit Clock buffer output
    		I => ref_200_clk_s -- 1-bit Clock buffer input
    	);
    	
    	
    	--2. DRY path
    	
    	-- -----------buffer for DRY--------
    	IBUFGDS_inst_clk1 : IBUFGDS
    	generic map (
    	DIFF_TERM => FALSE, -- Differential Termination
    	IBUF_LOW_PWR => TRUE, -- Low power (TRUE) vs. performance (FALSE) setting for refernced I/O standards
    	IOSTANDARD => "DEFAULT")
    	port map (
    		O => dry_clk_s, -- Clock buffer output
    		I => dry_clk_inp, -- Diff_p clock buffer input (connect directly to top-level port)
    		IB => dry_clk_inn -- Diff_n clock buffer input (connect directly to top-level port)
    	);
    	
    	
    	
    	--	-------------IODELAY for DRY------------------
    	
    	-- This IDELAY has : input  = dry_clk_s , output = dry_clk_delayed_s, clock = clk_for_delay, inc, rst, en = need to find out
    	
    	
       IODELAYE1_inst_clk1 : IODELAYE1
    	generic map (
          CINVCTRL_SEL => FALSE,         -- Enable dynamic clock inversion ("TRUE"/"FALSE") 
          DELAY_SRC => "I",                -- Delay input ("I", "CLKIN", "DATAIN", "IO", "O")
          HIGH_PERFORMANCE_MODE => TRUE, -- Reduced jitter ("TRUE"), Reduced power ("FALSE")
          IDELAY_TYPE => "FIXED",        -- "DEFAULT", "FIXED", "VARIABLE", or "VAR_LOADABLE" 
          IDELAY_VALUE => 20,               -- Input delay tap setting (0-32)
    -- v2.13 made idelay value =2 
          ODELAY_TYPE => "FIXED",          -- "FIXED", "VARIABLE", or "VAR_LOADABLE" 
          ODELAY_VALUE => 0,               -- Output delay tap setting (0-32)
          REFCLK_FREQUENCY => 200.0,       -- IDELAYCTRL clock input frequency in MHz
          SIGNAL_PATTERN => "DATA"         -- "DATA" or "CLOCK" input signal
       )
       
    			
       port map (
          CNTVALUEOUT => open , -- 5-bit output - Counter value for monitoring purpose
          DATAOUT => dry_clk_delayed_s,       -- 1-bit output - Delayed data output
          C => Low,                     -- 1-bit input - Clock input
          CE => Low,                   -- 1-bit input - Active high enable increment/decrement function
          CINVCTRL => Low,       -- 1-bit input - Dynamically inverts the Clock (C) polarity
          CLKIN => Low,             -- 1-bit input - Clock Access into the IODELAY
          CNTVALUEIN => LowWord,   -- 5-bit input - Counter value for loadable counter application
          DATAIN => Low,	          -- 1-bit input - Internal delay data
          IDATAIN => dry_clk_s ,      -- 1-bit input - Delay data input
          INC => Low,                 -- 1-bit input - Increment / Decrement tap delay
          ODATAIN => Low,         -- 1-bit input - Data input for the output datapath from the device
          RST => rst, -- 10.1                 -- 1-bit input - Active high, synchronous reset, resets delay chain to IDELAY_VALUE/
                                      -- ODELAY_VALUE tap. If no value is specified, the default is 0.
          T => High                      -- 1-bit input - 3-state input control. Tie high for input-only or internal delay or
                                      -- tie low for output only.
    
       );
    	
    
    	
    	MMCM_BASE_inst_1 : MMCM_BASE
    	generic map (
    	BANDWIDTH => "OPTIMIZED", -- Jitter programming ("HIGH","LOW","OPTIMIZED")
    	
    	CLKFBOUT_MULT_F => 16.0, -- v3.1 v4.1
    	CLKFBOUT_PHASE => 0.0, -- Phase offset in degrees of CLKFB (0.00-360.00).
    
    	CLKIN1_PERIOD => 20.833, -- v3.1   48kHz)		-- v4.1
    	CLKOUT0_DIVIDE_F => 1.0, -- Divide amount for CLKOUT0 (1.000-128.000).
    	
    	CLKOUT4_DUTY_CYCLE => 0.5,
    	
    	CLKOUT4_PHASE => 0.0,
    	
    	CLKOUT4_DIVIDE => 8, --v3.1
    	CLKOUT4_CASCADE => FALSE, -- Cascase CLKOUT4 counter with CLKOUT6 (TRUE/FALSE)
    	CLOCK_HOLD => FALSE, -- Hold VCO Frequency (TRUE/FALSE)
    
    	DIVCLK_DIVIDE => 1, -- Master division value (1-80) -- v4.1
    					-- 5 so that 250 Mhz * (5/5) = 250 Mhz Version 1.2
    	REF_JITTER1 => 0.0, -- Reference input jitter in UI (0.000-0.999).
    	STARTUP_WAIT => FALSE -- Not supported. Must be set to FALSE.
    	)
    
    	port map (
    	
    	CLKOUT4 => clkout4pin_1, -- 1-bit output: CLKOUT0 output
    	
    	CLKFBOUT => CLKFBOUTpin_1, -- 1-bit output: Feedback clock output
    	CLKFBOUTB => CLKFBOUTBpin_1, -- 1-bit output: Inverted CLKFBOUT output
    	
    	LOCKED => Led_1, -- 1-bit output: LOCK output
    	
    	CLKIN1 => dry_clk_delayed_s, -- 2.13
    	
    	PWRDWN => PWRDWN, -- 1-bit input: Power-down input
    	RST =>  RST, -- 1-bit input: Reset input
    	-- Feedback Clocks: 1-bit (each) input: Clock feedback ports
    	CLKFBIN => CLKFBINpin_1 -- 1-bit input: Feedback clock input
    	);
    	
    	-- ----------Bufg for fback ---------------------
    	-- version 1.1
    	BUFG_inst_1 : BUFG
    	port map (
    	O => clkfbinpin_1, -- 1-bit output: Clock buffer output
    	I => clkfboutpin_1 -- 1-bit input: Clock buffer input
    	);
    
    
    -- ------- bufg for dry_clk_2x ------------------
    	-- version 1.1
    	BUFG_inst11 : BUFG
    	port map (
    	O => dry_clk_2x, -- 1-bit output: Clock buffer output
    	I => clkout4pin_1 -- 1-bit input: Clock buffer input
    	);
    			
    		
    	
    	
    	-- 3. ADC inputs
    	
    	---------- ADC data input to FPGA -------------------
    	ADC_IN_GEN: for j in 0 to 11 generate
    	begin
    
    	IBUFDS_inst_IO_DA : IBUFDS
    	generic map (
    		DIFF_TERM => FALSE, -- Differential Termination
    		IBUF_LOW_PWR => TRUE, -- Low power (TRUE) vs. performance (FALSE) setting for refernced I/O standards
    		IOSTANDARD => "DEFAULT")
    		port map (
    			O => adc_data_s(j),
    			I => adc_inp(j),
    			IB => adc_inn(j)
    		);
    		
    	IODELAYE1_inst : IODELAYE1
    	generic map (
    		CINVCTRL_SEL => FALSE,         -- Enable dynamic clock inversion ("TRUE"/"FALSE") 
    		DELAY_SRC => "I",                -- Delay input ("I", "CLKIN", "DATAIN", "IO", "O")
    		HIGH_PERFORMANCE_MODE => TRUE, -- Reduced jitter ("TRUE"), Reduced power ("FALSE")
    		IDELAY_TYPE => "DEFAULT",        -- "DEFAULT", "FIXED", "VARIABLE", or "VAR_LOADABLE" 
    		IDELAY_VALUE => 0,               -- Input delay tap setting (0-32)
    		ODELAY_TYPE => "FIXED",          -- "FIXED", "VARIABLE", or "VAR_LOADABLE" 
    		ODELAY_VALUE => 0,               -- Output delay tap setting (0-32)
    		REFCLK_FREQUENCY => 200.0,       -- IDELAYCTRL clock input frequency in MHz
    		SIGNAL_PATTERN => "DATA"         -- "DATA" or "CLOCK" input signal
    	)
    	port map (
    		CNTVALUEOUT => open , -- 5-bit output - Counter value for monitoring purpose
    		DATAOUT => data_delayed_s(j),       -- 1-bit output - Delayed data output
    		C => Low,                     -- 1-bit input - Clock input
    		CE => Low,                   -- 1-bit input - Active high enable increment/decrement function
    		CINVCTRL => Low,       -- 1-bit input - Dynamically inverts the Clock (C) polarity
    		CLKIN => Low,             -- 1-bit input - Clock Access into the IODELAY
    		CNTVALUEIN => LowWord,   -- 5-bit input - Counter value for loadable counter application
    		DATAIN => Low,	          -- 1-bit input - Internal delay data
    		IDATAIN => adc_data_s(j) ,      -- 1-bit input - Delay data input
    		INC => Low,                 -- 1-bit input - Increment / Decrement tap delay
    		ODATAIN => Low,         -- 1-bit input - Data input for the output datapath from the device
    		RST => rst, -- 10.1                -- 1-bit input - Active high, synchronous reset, resets delay chain to IDELAY_VALUE/
                                      -- ODELAY_VALUE tap. If no value is specified, the default is 0.
    		T => High                      -- 1-bit input - 3-state input control. Tie high for input-only or internal delay or
                                      -- tie low for output only.
    
    	);
    	
       FF_inst : FDCE
            generic map (INIT => '0')
            port map (D => data_delayed_s(j), CE => not rst, C => dry_clk_2x, CLR => Low,
                      Q => ff_data(j));
    						
    end generate ADC_IN_GEN;
    
    
    
     -- 4. fpga clock from DAC
    
    
    	-- -------------------buffer for fpga_clock from DAC------------------------------------------------
    	IBUFGDS_inst2 : IBUFGDS
    	generic map (
    	DIFF_TERM => FALSE, -- Differential Termination
    	IBUF_LOW_PWR => TRUE, -- Low power (TRUE) vs. performance (FALSE) setting for refernced I/O standards
    	IOSTANDARD => "DEFAULT")
    	port map (
    		O => fpga_clk_s, -- Clock buffer output
    		I => fpga_clk_inp, -- Diff_p clock buffer input (connect directly to top-level port)
    		IB => fpga_clk_inn -- Diff_n clock buffer input (connect directly to top-level port)
    	);
    
     process (led_1, led_2) begin
     if (led_1 = '1') and (led_2 = '1') then
      fifo_rst <= '0';
     else
    	fifo_rst <= '1';
    end if;
    
    end process;
    
    -- for write edge, if fifo_rst = 0 wr_en = 1 else wr_en = 0
     -- wr_en = wr_en
     
     process (dry_clk_2x) begin
     if (rising_edge(dry_clk_2x)) then
      if (fifo_rst = '0') then
    		wr_en_in <= '1';
    	else
    		wr_en_in <= '0';
    	end if;
    else
    	wr_en_in <= wr_en_in ;
    end if;
    end process;
    
    
    process (data_clk) begin
     if (rising_edge(data_clk)) then
      if (fifo_rst = '0') then
    		rd_en_in <= '1';
    	else
    		rd_en_in <= '0';
    	end if;
    else
    	rd_en_in <= rd_en_in ;
    end if;
    end process;		
    
    
    -- v2.10 ends
    fifo_inst1 : fifo_generator_v9_3
      PORT MAP (
        rst => fifo_rst,
        wr_clk => dry_clk_2x,
        rd_clk => data_clk,
        din => ff_data,
        wr_en => wr_en_in,
        rd_en =>rd_en_in,
        dout => fifo_out,
        full => full,
        wr_ack => wr_ack,
        overflow => overflow,
        empty => empty,
        valid => valid,
        underflow => underflow
      );							
    						
    						
    	---------------------------------------------- Idelay Control ----------------------------------------------------------------------
    	
    	IDELAYCTRL_inst : IDELAYCTRL
    		port map (
    			RDY => Ready_idelay_out, -- 1-bit output indicates validity of the REFCLK
    			REFCLK => ref_clk200_bufg, -- 1-bit reference clock input
    			RST	=> rst -- 10.1 -- 1-bit reset input
    		);
    	
    	
    MMCM_BASE_inst : MMCM_BASE
    	generic map (
    	BANDWIDTH => "OPTIMIZED", -- Jitter programming ("HIGH","LOW","OPTIMIZED")
    	-- v 2.15 CLKFBOUT_MULT_F => 15.0, -- Multiply value for all CLKOUT (5.0-64.0).
    	CLKFBOUT_MULT_F => 16.0, -- Multiply value for all CLKOUT (5.0-64.0). --2.15
    	CLKFBOUT_PHASE => 0.0, -- Phase offset in degrees of CLKFB (0.00-360.00).
    	
       CLKIN1_PERIOD => 10.416, -- v4.1 Input clock period in ns to ps resolution (i.e. 33.333 is 30 MHz).(or 21.7 if input freq is 46.08 msps) or 86.8			
    			-- 4 ns = 250 MHz Version 1.2
    	CLKOUT0_DIVIDE_F => 2.0, --  Divide amount for CLKOUT0 (1.000-128.000). -- v2.15
    	-- CLKOUT0_DUTY_CYCLE - CLKOUT6_DUTY_CYCLE: Duty cycle for each CLKOUT (0.01-0.99).
    	CLKOUT0_DUTY_CYCLE => 0.5, -- v2.14
    	
    	CLKOUT4_DUTY_CYCLE => 0.5,
    	-- CLKOUT0_PHASE - CLKOUT6_PHASE: Phase offset for each CLKOUT (-360.000-360.000).
    	CLKOUT0_PHASE => 0.0, -- v2.14
    	CLKOUT4_PHASE => 0.0,
    	
    		CLKOUT4_DIVIDE => 8, -- v2.15 -- v4.1
    	CLKOUT4_CASCADE => FALSE, -- Cascase CLKOUT4 counter with CLKOUT6 (TRUE/FALSE)
    	CLOCK_HOLD => FALSE, -- Hold VCO Frequency (TRUE/FALSE)
    	-- v2.15 DIVCLK_DIVIDE => 5, -- Master division value (1-80)
    	 DIVCLK_DIVIDE => 2, -- Master division value (1-80) -- v2.15 -- v4.1
    	-- DIVCLK_DIVIDE => 4, -- Master division value (1-80) -- v2.15
    						-- 5 so that 250 Mhz * (5/5) = 250 Mhz Version 1.2
    	REF_JITTER1 => 0.0, -- Reference input jitter in UI (0.000-0.999).
    	STARTUP_WAIT => FALSE -- Not supported. Must be set to FALSE.
    	)
    
    	port map (
    	-- Clock Outputs: 1-bit (each) output: User configurable clock outputs
    	CLKOUT0 => clkout0pin, -- 1-bit output: CLKOUT0 output -- v2.14
    	
    	CLKOUT4 => clkout4pin, -- 1-bit output: CLKOUT0 output
    	-- Feedback Clocks: 1-bit (each) output: Clock feedback ports
    	CLKFBOUT => CLKFBOUTpin, -- 1-bit output: Feedback clock output
    	CLKFBOUTB => CLKFBOUTBpin, -- 1-bit output: Inverted CLKFBOUT output
    	-- Status Port: 1-bit (each) output: MMCM status ports
    	LOCKED => Led_2, -- 1-bit output: LOCK output
    	-- Clock Input: 1-bit (each) input: Clock input
    	CLKIN1 => fpga_clk_s,
    	-- Control Ports: 1-bit (each) input: MMCM control ports
    	PWRDWN => PWRDWN, -- 1-bit input: Power-down input
    	RST =>  RST, -- 1-bit input: Reset input
    	-- Feedback Clocks: 1-bit (each) input: Clock feedback ports
    	CLKFBIN => CLKFBINpin -- 1-bit input: Feedback clock input
    	);
    
    
     ---------------------------------------------------Bufg for clkout0 ------------------------------------------------------------------
    	-- version 1.1
    	BUFG_inst_chip : BUFG
    	port map (
    	O => chip_780_clk, -- 1-bit output: Clock buffer output
    	I => clkout0pin -- 1-bit input: Clock buffer input
    	);
    
    -- ---------------------------------------------------Bufg for fback ------------------------------------------------------------------
    	-- version 1.1
    	BUFG_inst : BUFG
    	port map (
    	O => clkfbinpin, -- 1-bit output: Clock buffer output
    	I => clkfboutpin -- 1-bit input: Clock buffer input
    	);
    
    
    -- --------------------------------------------------- bufg for data_clk ------------------------------------------------------------------
    	-- version 1.1
    	BUFG_inst1 : BUFG
    	port map (
    	O => data_clk, -- 1-bit output: Clock buffer output
    	I => clkout4pin -- 1-bit input: Clock buffer input
    	);
    	
    	data_clk1<= data_clk;
    						
    	
    
    		
    counter_dataclk : counter1 port map (fpga_clk_s, led_out2, '0');
    --counter_dataclk_2x : counter1 port map (dry_clk_2x, led_out3, '0');	
    counter_dataclk_2x : counter1 port map (IO_DA(6), led_out3, '0');
    
     led_out (7 downto 5) <= led_out2 (7 downto 5);
     led_out (4 downto 2) <= led_out3(7 downto 5);
    --led_out(7 downto 2) <= adc_data_s(7 downto 2);
    
    led_out (1)	<= Led_2; -- fpga clock
    led_out	(0) <= Led_1; -- write clock
    
    -- 2.11 starts
    
    IO_DA(15 downto 4) <= fifo_out;
    IO_DA (3 downto 0) <= "0000";
    	 --------------------------------- output buffer for outputs to DAC-------------------------------------------------------
    	 IO_DA_GEN: for j in 0 to 15 generate
    	 begin
    	 OBUFDS_inst_IO_DA : OBUFDS
    	 generic map (
    	 IOSTANDARD => "DEFAULT")
    	 port map (
    		 O => IO_DAP(j),
    		 OB => IO_DAN(j),
    		 I => IO_DA(j)
    	 );
    	 end generate IO_DA_GEN;
    	-- ----------------------------------------------output buffer for data clock1 -------------------------------------------------------
    	OBUFDS_inst_dataclk : OBUFDS
    	generic map (
    	IOSTANDARD => "DEFAULT")
    	port map (
    		O => DATA_CLKP, -- Diff_p output (connect directly to top-level port)
    		OB => DATA_CLKN, -- Diff_n output (connect directly to top-level port)
    		I => DATA_CLK1 -- Buffer input
    	);
    
    	----------------------------------------------------------- output buffer for Parity-------------------------------------------------------
    	OBUFDS_inst_sync_PARITY : OBUFDS
    	generic map (
    	IOSTANDARD => "DEFAULT")
    	port map (
    		O => PARITYP, -- Diff_p output (connect directly to top-level port)
    		OB => PARITYN, -- Diff_n output (connect directly to top-level port)
    		I => PARITY -- Buffer input
    	);
    
    	--sync <= not sync;
    	-------------------------------------------------------------- output buffer for Sync-------------------------------------------------------
    	OBUFDS_inst_sync : OBUFDS
    	generic map (
    	IOSTANDARD => "DEFAULT")
    	port map (
    		O => SYNCP, -- Diff_p output (connect directly to top-level port)
    		OB => SYNCN, -- Diff_n output (connect directly to top-level port)
    		I => SYNC -- Buffer input
    	);
    
    	--fifo_istr <= not fifo_istr;
     	-------------------------------------------------------------- output buffer for FIFO_ISTR-------------------------------------------------------
    	OBUFDS_inst_FIFO : OBUFDS
    		generic map (
    	IOSTANDARD => "DEFAULT")
    	port map (
    		O => FIFO_ISTRP, -- Diff_p output (connect directly to top-level port)
    		OB => FIFO_ISTRN, -- Diff_n output (connect directly to top-level port)
    		I => FIFO_ISTR -- Buffer input
    	);
    	
    	-------------------- output buffer for sma_out to ADC clock ------------------
    	-- 1.3
    	OBUFDS_inst_sma : OBUFDS
    		generic map (
    		IOSTANDARD => "DEFAULT")
    		port map (
    			O => sma_outp, -- Diff_p output (connect directly to top-level port)
    			OB => sma_outn, -- Diff_n output (connect directly to top-level port)
    			I => data_clk -- Buffer input
    		);	
    	
    
    -- 2.11 ends 
    	
    	
    end Behavioral;
    
    
    # 2.11 starts
    NET "IO_DAP[15]" IOSTANDARD = LVDS_25;
    NET "IO_DAP[14]" IOSTANDARD = LVDS_25;
    NET "IO_DAP[13]" IOSTANDARD = LVDS_25;
    NET "IO_DAP[12]" IOSTANDARD = LVDS_25;
    NET "IO_DAP[11]" IOSTANDARD = LVDS_25;
    NET "IO_DAP[10]" IOSTANDARD = LVDS_25;
    NET "IO_DAP[9]" IOSTANDARD = LVDS_25;
    NET "IO_DAP[8]" IOSTANDARD = LVDS_25;
    NET "IO_DAP[7]" IOSTANDARD = LVDS_25;
    NET "IO_DAP[6]" IOSTANDARD = LVDS_25;
    NET "IO_DAP[5]" IOSTANDARD = LVDS_25;
    NET "IO_DAP[4]" IOSTANDARD = LVDS_25;
    NET "IO_DAP[3]" IOSTANDARD = LVDS_25;
    NET "IO_DAP[2]" IOSTANDARD = LVDS_25;
    NET "IO_DAP[1]" IOSTANDARD = LVDS_25;
    NET "IO_DAP[0]" IOSTANDARD = LVDS_25;
    
    
    
    #2.8 #2.11
    NET "DATA_CLKP" IOSTANDARD = LVDS_25;
    #2.8 #2.11
    NET "FIFO_ISTRP" IOSTANDARD = LVDS_25;
    #2.8
    NET "fpga_clk_inp" IOSTANDARD = LVDS_25;
    #2.8 #2.11
    NET "PARITYP" IOSTANDARD = LVDS_25;
    #2.8 #2.11
    NET "SYNCP" IOSTANDARD = LVDS_25;
    #2.8 #2.11
    NET "sma_outp" IOSTANDARD = LVDS_25;
    #2.8 #2.11
    NET "sma_outn" IOSTANDARD = LVDS_25;
    
    
    NET "IO_DAP[0]" LOC = AN30;
    NET "IO_DAP[1]" LOC = AN29;
    NET "IO_DAP[2]" LOC = AN25;
    NET "IO_DAP[3]" LOC = AM23;
    NET "IO_DAP[4]" LOC = AM22;
    NET "IO_DAP[5]" LOC = AK21;
    NET "IO_DAP[6]" LOC = AF19;
    NET "IO_DAP[7]" LOC = AC20;
    NET "IO_DAP[8]" LOC = AH23;
    NET "IO_DAP[9]" LOC = AL29;
    NET "IO_DAP[10]" LOC = AL28;
    NET "IO_DAP[11]" LOC = AN28;
    NET "IO_DAP[12]" LOC = AP27;
    NET "IO_DAP[13]" LOC = AK23;
    NET "IO_DAP[14]" LOC = AP22;
    NET "IO_DAP[15]" LOC = AM21;
    #2.8 2.11
    NET "DATA_CLKP" LOC = AH25;
    #2.8 2.11
    NET "FIFO_ISTRP" LOC = AG25;
    #2.8 2.11
    NET "FIFO_ISTRN" LOC = AG26;
    #2.8
    NET "fpga_clk_inp" LOC = K24;
    NET "fpga_clk_inn" LOC = K23;
    #2.8 2.11
    NET "PARITYP" LOC = AK27;
    #2.8 2.11
    NET "SYNCP" LOC = AJ24;
    #2.8 2.11
    NET "sma_outp" LOC = V34;
    #2.8 2.11
    NET "sma_outn" LOC = W34;
    #2.8NET "LED" LOC = AC22;
    #2.8NET "LED" IOSTANDARD = LVCMOS25;
    # 2.11 ends
    NET "rst" LOC = A19;
    NET "rst" IOSTANDARD = LVCMOS25;
    
    # 2.11 starts
    #NET "fifo_rst" LOC = A18;#2.8  pushbutton SW6
    #NET "wr_en_in" LOC = H17;#2.8  SW8
    #NET "rd_en_in" LOC = G17;#2.8 SW7
    #
    #NET "fifo_rst" IOSTANDARD = LVCMOS25;#2.8
    #NET "wr_en_in" IOSTANDARD = LVCMOS25;#2.8
    #NET "rd_en_in" IOSTANDARD = LVCMOS25; #2.8
    # 2.11 ends
    ##NET "led_clk" LOC = AC24;
    ## led 0 - DS12	#2.8
    NET "led_out[0]" LOC = AC22;
    NET "led_out[1]" LOC = AC24;
    NET "led_out[2]" LOC = AE22;
    NET "led_out[3]" LOC = AE23;
    NET "led_out[4]" LOC = AB23;
    NET "led_out[5]" LOC = AG23;
    NET "led_out[6]" LOC = AE24;
    ## led 8 - DS21
    NET "led_out[7]" LOC = AD24;
    #NET "led_clk" IOSTANDARD = LVCMOS25;
    #2.8
    NET "led_out[0]" IOSTANDARD = LVCMOS25;
    NET "led_out[1]" IOSTANDARD = LVCMOS25;
    NET "led_out[2]" IOSTANDARD = LVCMOS25;
    NET "led_out[3]" IOSTANDARD = LVCMOS25;
    NET "led_out[4]" IOSTANDARD = LVCMOS25;
    NET "led_out[5]" IOSTANDARD = LVCMOS25;
    NET "led_out[6]" IOSTANDARD = LVCMOS25;
    NET "led_out[7]" IOSTANDARD = LVCMOS25;
    ## ADC pin out
    #NET "adc_inp[0]" LOC = J31;
    #NET "adc_inn[0]" LOC = J32;
    #NET "adc_inp[1]" LOC = J30;
    #NET "adc_inn[1]" LOC = K29;
    NET "adc_inp[11]" LOC = G32;
    NET "adc_inn[11]" LOC = H32;
    NET "adc_inp[10]" LOC = E32;
    NET "adc_inn[10]" LOC = E33;
    NET "adc_inp[9]" LOC = D31;
    NET "adc_inn[9]" LOC = D32;
    NET "adc_inp[8]" LOC = A33;
    NET "adc_inn[8]" LOC = B33;
    NET "adc_inp[7]" LOC = C32;
    NET "adc_inn[7]" LOC = B32;
    NET "adc_inp[6]" LOC = M30;
    NET "adc_inn[6]" LOC = N30;
    NET "adc_inp[5]" LOC = P29;
    NET "adc_inn[5]" LOC = R29;
    NET "adc_inp[4]" LOC = N27;
    NET "adc_inn[4]" LOC = P27;
    NET "adc_inp[3]" LOC = R26;
    NET "adc_inn[3]" LOC = T26;
    NET "adc_inp[2]" LOC = N32;
    NET "adc_inn[2]" LOC = P32;
    NET "adc_inp[1]" LOC = P31;
    NET "adc_inn[1]" LOC = P30;
    NET "adc_inp[0]" LOC = C33;
    NET "adc_inn[0]" LOC = B34;
    #NET "adc_inp[0]" LOC = N33;
    #NET "adc_inn[0]" LOC = M33;
    
    #NET "ovr_inp" LOC = J30;
    #NET "ovr_inn" LOC = K29;
    
    NET "dry_clk_inp" LOC = N28;
    NET "dry_clk_inn" LOC = N29;
    NET "SYSCLK_P" LOC = J9;
    NET "SYSCLK_N" LOC = H9;
    NET "dry_clk_inp" CLOCK_DEDICATED_ROUTE = FALSE;
    NET "dry_clk_inn" CLOCK_DEDICATED_ROUTE = FALSE;
    
    NET "adc_inp[0]" IOSTANDARD = LVDS_25;
    NET "adc_inn[0]" IOSTANDARD = LVDS_25;
    NET "adc_inp[1]" IOSTANDARD = LVDS_25;
    NET "adc_inn[1]" IOSTANDARD = LVDS_25;
    NET "adc_inp[2]" IOSTANDARD = LVDS_25;
    NET "adc_inn[2]" IOSTANDARD = LVDS_25;
    NET "adc_inp[3]" IOSTANDARD = LVDS_25;
    NET "adc_inn[3]" IOSTANDARD = LVDS_25;
    NET "adc_inp[4]" IOSTANDARD = LVDS_25;
    NET "adc_inn[4]" IOSTANDARD = LVDS_25;
    NET "adc_inp[5]" IOSTANDARD = LVDS_25;
    NET "adc_inn[5]" IOSTANDARD = LVDS_25;
    NET "adc_inp[6]" IOSTANDARD = LVDS_25;
    NET "adc_inn[6]" IOSTANDARD = LVDS_25;
    NET "adc_inp[7]" IOSTANDARD = LVDS_25;
    NET "adc_inn[7]" IOSTANDARD = LVDS_25;
    NET "adc_inp[8]" IOSTANDARD = LVDS_25;
    NET "adc_inn[8]" IOSTANDARD = LVDS_25;
    NET "adc_inp[9]" IOSTANDARD = LVDS_25;
    NET "adc_inn[9]" IOSTANDARD = LVDS_25;
    NET "adc_inp[10]" IOSTANDARD = LVDS_25;
    NET "adc_inn[10]" IOSTANDARD = LVDS_25;
    NET "adc_inp[11]" IOSTANDARD = LVDS_25;
    NET "adc_inn[11]" IOSTANDARD = LVDS_25;
    NET "dry_clk_inp" IOSTANDARD = LVDS_25;
    NET "dry_clk_inn" IOSTANDARD = LVDS_25;
    NET "SYSCLK_P" IOSTANDARD = LVDS_25;
    NET "SYSCLK_N" IOSTANDARD = LVDS_25;
    
    #NET "ovr_inp" IOSTANDARD = LVDS_25;
    #NET "ovr_inn" IOSTANDARD = LVDS_25;
    
    
    
    # 2.11 : 11:40 pm 06 May
    #  -- This file is being used in adc_to_dac_1 project directory
    #  -- adc -> fpga -> dac is being written
    #  -- March 18 entry
    #Created by Constraints Editor (xc6vlx240t-ff1156-1) - 2014/05/07
    NET "dry_clk_inn" TNM_NET = "dry_clk_inn";
    TIMESPEC TS_dry_clk_inn = PERIOD "dry_clk_inn" 20.833 ns HIGH 50 %;
    NET "dry_clk_inp" TNM_NET = "dry_clk_inp";
    TIMESPEC TS_dry_clk_inp = PERIOD "dry_clk_inp" 20.833 ns HIGH 50 %;
    NET "fpga_clk_inn" TNM_NET = "fpga_clk_inn";
    TIMESPEC TS_fpga_clk_inn = PERIOD "fpga_clk_inn" 10.416 ns HIGH 50 %;
    NET "fpga_clk_inp" TNM_NET = "fpga_clk_inp";
    TIMESPEC TS_fpga_clk_inp = PERIOD "fpga_clk_inp" 10.416 ns HIGH 50 %;
    #Created by Constraints Editor (xc6vlx240t-ff1156-1) - 2014/05/07
    INST "adc_inn[0]" TNM = "data_in";
    INST "adc_inn[1]" TNM = "data_in";
    INST "adc_inn[2]" TNM = "data_in";
    INST "adc_inn[3]" TNM = "data_in";
    INST "adc_inn[4]" TNM = "data_in";
    INST "adc_inn[5]" TNM = "data_in";
    INST "adc_inn[6]" TNM = "data_in";
    INST "adc_inn[7]" TNM = "data_in";
    INST "adc_inn[8]" TNM = "data_in";
    INST "adc_inn[9]" TNM = "data_in";
    INST "adc_inn[10]" TNM = "data_in";
    INST "adc_inn[11]" TNM = "data_in";
    INST "adc_inp[0]" TNM = "data_in";
    INST "adc_inp[1]" TNM = "data_in";
    INST "adc_inp[2]" TNM = "data_in";
    INST "adc_inp[3]" TNM = "data_in";
    INST "adc_inp[4]" TNM = "data_in";
    INST "adc_inp[5]" TNM = "data_in";
    INST "adc_inp[6]" TNM = "data_in";
    INST "adc_inp[7]" TNM = "data_in";
    INST "adc_inp[8]" TNM = "data_in";
    INST "adc_inp[9]" TNM = "data_in";
    INST "adc_inp[10]" TNM = "data_in";
    INST "adc_inp[11]" TNM = "data_in";
    TIMEGRP "data_in" OFFSET = IN -0.25 ns VALID 10.1665 ns BEFORE "dry_clk_inp" RISING;
    TIMEGRP "data_in" OFFSET = IN -0.25 ns VALID 10.1665 ns BEFORE "dry_clk_inp" FALLING;
    TIMEGRP "data_in" OFFSET = IN -0.25 ns VALID 10.1665 ns BEFORE "dry_clk_inn" RISING;
    TIMEGRP "data_in" OFFSET = IN -0.25 ns VALID 10.1665 ns BEFORE "dry_clk_inn" FALLING;
    

    Thank you

    Pramod singh