This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS7863A 0V to 5V Input

Other Parts Discussed in Thread: ADS7863A

Hallo,

Can the ADS7863A be used in the input range of 0V to 5V?
Looking at Table 9 of the datasheet, it seems that the input full-scale range of CHxx+ is 5V when CHxx– = VREF = 2.5 V, and the output ‘7FF’ will be 5V and ‘800’ be 0V.
If possible to use CHxx+ as 5V full-scale single-end input,
Does it degrade the accuracy of the analog signal conversion to the digital?
Could you please advise me?

Best Regards,
Kazu Ogawa