Other Parts Discussed in Thread: ADS1256, ADS1282, OPA1632
Hi i am using the ads1282 evm with an arm microcontroller which i had used with an ads1256 evm previously.
i have now modified the program code quickly and all i get out of the ads1282 is FFFFFFFF as ADC Code.
i had also the problem that a cable on my power supply the 5 Volt positiv supply got off so i measured -1.6V on the analog input pin ,
now i think that maybe the ads1282 modulator is destroyed, thats why i ask you if this could be the case, also i measured 50 mA on the postiv supply as current draw and
the ads1282 gets slightly warm (about 35°C)
Can the ADS1282 be broken ? What can i check? I think i will now put a scope on the direct modulator output to see whats happening?
Thank you in advance for your answer.
Ralph Reiter
E-Mail: ralph.reiter@uni.lu