Hello,
I have a question on the ADS1248. We have the device working but the readings we are getting are much lower then expected. When I change the gain the readings change by the expected ratio, e.g. 128 is twice the hex code as 64. I am running a 4 wire RTD that will be reading from -80 C to 300 C. So I need approximately 128 mV at full scale. I am using the internal reference so 128 mV with a gain of 16 should be very close to full scale even with offset errors. I currently have a precision POT in place of my RTD so I can adjust the input. I have a DMM across my pot to read the voltage. The code I am getting at 128 mV input is 0x0E7670 with a gian of 16. So about 1/8 of full scale. Changing my gain I get the readings below:
Gain HEX output
128 3B9679
64 1DCAC5
32 0EE699
so these seem to be the correct ratio between gains but no where near the magnitude they should be. I can turn the pot up to around 400 mV and the code will rise with it until I saturate and get 7FFFFF. The other issue is that a gain of 32 and 16 give almost the same code. I have included a rough schematic of what I am working with.
Thanks for your help.
Jeff