Other Parts Discussed in Thread: ADS1298
I have two questions.
1) I believe the Sigma delta ADC can be configured for either unipolar or bipolar. Could someone tell me how to configure that. If it is unipolar how does it measure PQRST ECG signal (Negative part of the ECG wave) ?
2) Also about the ADC (digital count format).
I mean if IN1P is fed with 1mV DC and IN1N = 0V, and VREFP is at 2.4V , VREFN @ 0V. How much will ADC count?
For the same input of 1mV, how much will be the ADC counts when configured in bipolar mode?