Other Parts Discussed in Thread: ADCPRO, ADS1274, ADS1256, ADS1255
Hi Greg
I have posted this as a new question as I did not get a reply. Yes I would be very interested in the beta software for the ADCpro and ADS1256EVM. At this time I am using the ADS1271EVM and MMB0 boards. In the past I have used the ADS1210 ADC driven by a AD620 instrumentation amplifier from a 350ohm bridge load cell and it worked very well. Now I want to up the performance of that arrangement. (Target spec is +-19 bits noise free at 1kHZ) My development system at this time is the ADS1271EVM and MMB0 board driven by a INA2128 instrumentation amplifier with low pass filters. The ADS1271sample speed at this time is 20KSPS in Hi Res mode and are post filtering the ADC data but the noise is still to high. I have now obtained an ASD1274EVM board so I can use it with the ADCpro software to check my current noise results. Before I stop development on the ADS1271 /ADS1274 arrangement, I would like to try other ADC's and compare results. Any suggestions to help me reach my target will be a great help.
Kind regards
John Ivory.