Other Parts Discussed in Thread: THS4521, ADS5240, ADC3422
Hello
My customer intends to use ADC for IF sigal sampling
RF(470-810MHz)-->Discrete Down Convert to IF(10.2MHz) ---Amp(THS4521) --- ADC---Cyclone 4
*Requirements
-10bit or 12bit
-#2(2pcs) or #4ch(1pcs)
-40MHz
-Serial LVDS interface
-SNR >60dB
Current candidate
1st AD9219(ADI) with 3.3V to 1.8V LDO
http://www.analog.com/static/imported-files/data_sheets/AD9219.pdf
2nd
ADS5240 but, 12bit is too rich for their design.
So, 10bit /LVDS I/F /40MHz is required
3rd ADC10D40 but Parallel interface
4th ADC3422 but there are no 10bit version
**
Q1 Do you have ADC324x 10bit version road map?
Q2 Woulr you please advise about any counter plan to ADI's AD9219?
Customer knows that they should have 1.8V LDO but its easy....
**
With My Best Regards