Hello,
So I have a PCB with ADS1118's each reading 2 thermocouples and communicating via SPI with a CC2530. I had 4 prototypes that I know worked well Monday morning. When I tried testing them on Monday afternoon, they all had the same issue. The ADS1118 output no longer responds to the thermocouples. They constantly read either a near negligible reading or a reading that corresponds to around 3 degrees C. The on-board temperature sensor works just fine.
I checked the SPI communication and was able to verify that the ADC's were receiving the proper command, and verified that the values that I was receiving on my PC correlated to the values sent from the ADC's. Furthermore, I checked the inputs to the ADC and verified that the thermocouples do operate properly. They just aren't being read properly.
So at this point, I've concluded that something is wrong with the ADC's themselves. However, this is 4 separate units that all went bad at the same time. Even worse, I tried replacing the ADC's on one with some spares I had in my desk. Unfortunately the problem persisted. What am I missing? Could something have happened to fry the ADC portion of all of these chips at once?
Any suggestions as to what to check or what the issue might be would be greatly appreciated.
Thanks,
Jon