Hello, I have designed a circuit using TLC7524 in BDAC (voltage) mode. I have run some test results already with a test bench circuit and the results were promising.
How ever I would like your opinion of my design if I may.
I am using 5V (buffered) reference and 10V (buffered) supply voltage. After the buffer amp I am getting 0.293V - 5V output, which is fine for me. Sorry about the messy schematic view.
I chose this model and mode, because I don't want to play with negative voltages and I have +3.3V 8 bit input, which is used without CS/WR. Original idea was to use 20V reference voltage, but I figured out that the supply voltage needs to be higher than the reference voltage and higher reference voltages would require higher input voltages. This may be obvious to you, but it should have been said in the datasheet.
So what do you think of this?