Hi
I am trying to interface ADS1294 with STM32F4 using SPI.
The problem is, that when I try to read the ID register, I allays get some different (wrong) value.
Here is my code:
void ads_read_from_register(adsRegister_t start_reg,
uint8_t number_of_reg_to_read, uint8_t *return_buff) {
uint16_t i, p;
CS_ADS_LOW;
//send SDATAC command
SPI_tx_rx_8bit(ADS_SPI, ADS_SDATAC);
//send RREG command and start address
SPI_tx_rx_8bit(ADS_SPI, (ADS_RREG | start_reg));
//send number of registers to read
SPI_tx_rx_8bit(ADS_SPI, (number_of_reg_to_read - 1));
for (i = 0; i < number_of_reg_to_read; i++) {
return_buff[i] = SPI_tx_rx_8bit(ADS_SPI, 0);
}
CS_ADS_HIGH;
}
void ads_init(void) {
uint32_t i;
//SPI initializations
ads_low_level_init();
i = 9000000;
while (i--)
; //wait
//activate ads1294
ADS_nPWDN_HIGH;
ADS_nRESET_HIGH;
i = 9000000;
while (i--)
; //wait
//perform reset
ADS_nRESET_LOW;
i = 9000000;
while (i--)
; //wait
ADS_nRESET_HIGH;
ADS_START_HIGH;
ads_read_from_register(ID, 20, &ads_reg[0]);
}
As you can see from above:
* nRESET is HIGH
* nPWDN is HIGH
* START is HIGH
* I want to use the internal clock of the chip so i set CLKSEL also to HIGH (this is done in the ads_low_level_init() )
* before i send RREG command i send SDATAC command
* in the next byte I send the number of registers to read -1
* after that a send number of registers to read -1 bytes in order to get the register content
As mentioned above the read value of the ID register is aways different.
I also checked the nDRDY line - I see peeks with period of 4ms so I guess the chip is running.
Please check also the scope screen shot

SPI configuration:
* CPOL=0 CPHA=1
* f_sclk = 10.5 MHz
best regards,
Stefan