Other Parts Discussed in Thread: ADS6425, ADS900, ADS800, ADS5294, ADS5263
Hi,
I have look at the datasheet of ADS644 and ADS6425 to check if it is possible to used either in the single-input configuration. But did not find any information on single-input configuration. want to used the single-input configuration with an analog input of 1.5Vpp. Need help with a reference circuit for either of these ADC in the single-input configuration.