Hi.
I am using ADC12D1000CIUT/NOPB ADC in my Design and The clock input to ADC is from LMX2581 clock synthesizer (Configuring for 1 GHz).
I want to know the sequence to be followed to run on-command calibration.
Like whether
1.clock synthesizer should be configured first then the on-command calibration or
2.clock synthesizer should be configured after the on-command calibration.
Also whether the input clock to ADC is required to run the on command calibration?
Regards,
Anil M