Hi, I have been testing the ADS1298 for a while, and while reading the docuemntation, I found a couple of things, that I think are typos:
- In the official datasheet ( http://www.ti.com/lit/ds/symlink/ads1298.pdf ), on page 22, Table9, the reset value for the CONFIG2 register appears as 0x40, but reading the description of the CONFIG2 register on page 25, I think that the reset value should be 0x00.
- In the document "Improving Common-Mode Rejection Using the Right-Leg Drive Amplifier" ( http://www.ti.com/lit/an/sbaa188/sbaa188.pdf ), on page 7, there is a reference to "ADS1298ECGFE-PDK User's Guide", ( http://www.ti.com/lit/ug/sbau171c/sbau171c.pdf ), and in Figure 7, the input capacitors to the EVM are 47nF, but in the schematic on page 56 of the user guide document, the input capacitors are 47pF. ¿Which is the correct value?
Thank you and best regards,
Ariel Quezada