This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ads1672 sclk vs. sample clock

Other Parts Discussed in Thread: ADS1672

I plan to use the ADS1672 in an application with multiple sample rates, so the main clock on the ADS1672 will vary from 15 MHz to 2.5 MHz.  If I use an external SCLK for the SPI interface, are there any issues if SCLK is faster than the main ADC clock? For simplicity, I'm planning to operate my SPI bus at the rate for my fastest sample rate for all ADC sample rates.  As long as my SCLK and other SPI parameters are within the parameters listed in the table after Figure 2 in the data sheet, regardless of what the main ADC clock rate is, will this be ok?  Are there any issues I'm not considering?


Thanks,

Tobyn