Hello,
I'd like to measure currents from the low fA range up to 1 pA. It seems that the DDC114 could fit, if I understand the documentation correctly. What is the noise level I could expect with the longest integration time possible (1s)? According to the DDC114 datasheet on range 0 with a 50 pF load the noise would be 36 ppm FSR = 36e-6*12 pC=0.43e-15C, i.e. 1 pA for the given 400 us integration time. Is this noise independent of the integration time, i.e. would I get 430 aA total noise with 1 s integration time? Is it possible to further increase the integration time beyond 1s? Is there maybe a better component for this application? The measurement bandwidth is around 0.01 Hz.
Daniel