I am looking at the ADS1243 or ADS1248 for use in a weigh scale. The question is how low can we get the power for 2 SPS on 4 half (or full) bridge Load Cells. I do want to have some over sample / decimation to improve noise but I think we can get away with 8 or 16. I will be running this on 2500 mAhr rechargeable batteries and would like to get 3 to 6 months out of a charge. By the way there is WIFI on this so expect 4 to 6 < 1min transmissions per day at say 250 mA on average. If we could get the average current down to 300uA I think it could be accomplished. We are using a MSP430 as the controller so power is pretty low here.
Is this possible?
Thanks,