Other Parts Discussed in Thread: DAC34H84, DAC3482
Hello,
we need a 16 bit dual channel DAC with a real sampling rate of 600 Ms/s.
The DAC3482 seems adequate, but it requires a 1200 MHz data input rate (DDR), as it is equipped with a single input bus for both channels. In order to reduce this input rate, it is possble to use the DAC34H84 using the two input bus at 600 MHZ rate each, connected to a sigle couple of outputs (leaving the other two outputs unused)?
Excluding JESD204 devices, there is any alternative with dual 16 bit LVDS input bus?
Best regards,
Federico Cecili