Other Parts Discussed in Thread: ADS1293
HI Sir /Madam,
This is vengat here from Avnet India , one of my customer planning to do BLE based 3 Lead ECG Application .
They do have below Query , can you please revert back with feedback ASAP .
1. Possible gain setting available
2. Can we use fourth analog channel both for Pace detection and RLD ?
3. Whether AFE is compliant with regulatory standard like IEC 60601-1, IEC 60601-2-25, IEC 60601-2-27, IEC 60601-2-47
4. Actual power consumption while using at higher sampling rate (1000 sample/second/channel).
Thanks in Advance .
Rgds/
Vengat.