Other Parts Discussed in Thread: LM35, ADS1014
Hi,
I am currently usign a ADS1014 in differential mode to monitor temperature which is given by a lm35 in single supply mode.
The problem is that the value I read from the conversion register is always 0xFF70 until I reach about 1 - 1.2V then the values I read are in the range of 0xC0A0 like I am in the negative range of value.
The thing I don't understand is why even if AIN0-AIN1 in positive the values I read are in negative and why at 240mV the ADC stick at 0xFF70 which is the absolute positive value.
Thanks
Ben